How can we help you today?

What are the repair parts for a QMB322TD, series D2 (D02)?

Product Line:
QMB Switches

Resolution:
The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly - 4056669451 (1 required)
Load Base Assembly - 4056002550K (1 required; includes lugs)
Load Base Mounting Screw - 2142717161 (1 required per load base)
Handle Knob Kit - 4028343750
Lug Assembly - 4025101652 (per lug)
Lug Mounting Nut - 2342501701

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings