How can we help you today?

What are the repair parts for the H462, series F1? (may be shown as F01).

Product Line:
Safety Switches

Resolution:
The repair parts for the H462, series F1 (F01) are as follows. No other parts are available.
Interior kit - HSIF4606F (includes line and load base assemblies, arc suppressor, mechanism, mounting hardware, and instructions)
Load base kit - HLB2606F (2 required; includes load base, mounting hardware, and instructions)
Arc suppressor kit - HAS0610F (2 required; includes arc suppressor, mounting hardware, and instructions)
Lug kit - AL0306F (2 required; includes 6 lugs, mounting hardware, and instructions)
Handle/mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware, and instructions)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings