Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will the I-line panel accept a QO breaker?

Article available in these languages: Spanish

Issue:
Can QO breakers be mounted in an I-line panel?

Product Line:
Panelboards

Resolution:
Yes, by using a QO distribution panel rated for 240 V and below. They will all accept 30 A max breakers and have 6 spaces for QO plug on breakers. They take 4.5" of mounting space. The following items are available.
HQO306 - 3 phase
HQO206AB - single phase, AB phasing
HQO206AC - single phase, AC phasing
HQO206BC - single phase, BC phasing
See 48040-902-02

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings