Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do NEMA 1, 20`` wide X 5.75`` deep, MH type panel boxes come with blank endwalls as standard?
Issue:
Do MH boxes have blank or knockout end walls?

Product Line:
Panelboards

Environment:
NA

Cause:
Feature

Resolution:
The boxes have knockouts on one end and the other end is blank.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings