Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the torque for the MLO lug set-screw and lug bolt 1000A HCW2353-12?
Issue:
Torquing connections

Product Line:
Panelboards

Environment:
NA

Cause:
Install / Maintenance

Resolution:
Lug set screw - 340 in/lbs.
1/2`` KEPS nut w/ al terminals:  #2 - 600MCM CU-AL (1/2`` socket) - 38 ft lbs.
1/2`` KEPS nut w/ cu terminals:  #2 - 600MCM CU-AL (3/8`` socket) - 25 ft lbs.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings