Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is the SDSA1175 UL Listed as a Transient Voltage Surge Suppressor or as a Secondary Surge Arrestor?

The current design of SDSA1175 (Series 001) is UL Listed as a Transient Voltage Surge Suppressor, per UL 1449. It is also UL Listed as a Secondary Surge Arrestor, per ANSI/IEEE C62.11. It is marked for the Secondary Surge Arrestor application only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings