Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the date code of the Powerpact P or R matter if the trip unit will be replaced?

Issue:

Does the date code of the PowerPacT P or R matter if the trip unit will be replaced?

Product Line:

PowerPacT P and R Molded Case Circuit Breakers

Resolution:

Yes. Newly released trip units will not work on circuit breakers with date code 09011 (manufactured in the 1st week of 2009) or earlier. There are two options as a workaround:

·        Find a trip unit with date code 09011 or earlier

·        Replace the circuit breaker.

Visit this FAQ on how to locate the date code on PowerPacT breakers.
Visit this FAQ n how to locate the date code on Micrologic trip units.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings