Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What causes ATS480 PHF2 Faults

Resolution:

This fault usually occurs when the Mains Supply phase direction is not recognized when the
soft start is told to run. Would suggest to measure L1, L2 and L3 at the soft start. Ensure that
the control supply and mains is pulled in with or prior to a run command.  A time-delay in the
run circuit may be required for this.

Could also check the mains supply wiring and verify the Mains supply connection and any devices
located between the Mains and the soft start (Ex: Fuses, Contactor and/or circuit breakers).

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings