How can we help you today?

How can the ATS48 be switched from Modbus control to terminal control using one of its logic inputs?

Issue

How can a logic input be used to switch the ATS48 from Modbus to terminal control?

Product Line

ATS48

Environment:

Modbus Communication

Resolution:

Yes, can use LI3=LIL.

With LI3 = LIL (local forcing enabled):

  • When LI3 is closed -> the ATS48 takes commands from the terminal.
  • When LI3 is open and there are no Modbus requests -> the ATS48 takes commands from the terminals
  • When LI3 is open and there are Modbus requests -> the ATS48 takes commands from Modbus

In summary: The LI3 input in LIL mode allows forcing local control (via terminals) when it is closed or when it's open & Modbus is absent. As soon as Modbus is actively communicating and LI3 open, it takes priority.

See diagram below :

Diagram

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings