Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
Wiring of RS485 Communications Networks

Issue This document attempts to explain correct methods of wiring RS485 communication networks in industrial environments based on various application notes and technical articles. Environment RS485...

How to calculate necessary Air flow for cabinet cooling using Altivar...

The most precise method for calculating heating/cooling system for cabinet is to use dedicated software for cabinet thermal calculation. ProClima software is available on schneider web. Besides that,...

Cách kết nối CAPE ADVC3 với WSOS trên PC?

Có 3 cách để kết nối nộ Cape ADVC3 với PC thông qua phần mềm WSOS: 1. Kết nối thông qua cổng USB: + Cài lại phần mềm WSOS 5.16.13 theo link đính kèm bên dưới:...

PowerLogic PM5000 Series (PM51xx, PM53xx, PM55xx, PM56xx) Modbus Register...

Issue Register list for Modbus communication Product Line PM5110, PM5330, PM5340, PM5560, PM5563, PM56xx, PM57xx Environment Power Meter Communications Modbus Register List Cause PM5000 series...

PowerChute support with USB or Serial communication - Supported APC UPS...

Issue: When manually selecting an APC UPS during PowerChute Serial Shutdown or PowerChute Business Edition installation, multiple categories must be considered. Product Line: PowerChute Serial...

Data Center Expert | Working with SSL Certificates (Self-Signed, CSR, & CA...

Issue Working with self-signed and CA authority signed SSL certificates for the StruxureWare Data Center Expert appliance. Product Line StruxureWare Data Center Expert (DCE) - Basic Appliance...

How do I upgrade the firmware on an APC Network Management Card (NMC) or...

Issue You wish to upgrade your Network Management Card's (NMC) firmware or have been instructed to. You have a device such as a Smart-UPS, Smart-UPS Ultra, Easy UPS On-Line, Easy UPS 3-Phase,...

Troubleshooting "Application is incompatible with this AOS" messages on a...

Issue: When logging into the web interface of a Network Management Card (NMC), the user is presented with an error message that the "Application is incompatible with this APC AOS" Product:...

Show more
Popular Video FAQsPopular Videos
Show more
Learn more through our Generic Knowledge FAQsGeneral Knowledge
Why is Neutral and Earth (Ground) Connection forbidden Downstream from...

The question is often asked what is the maximum voltage permitted between the Neutral and Earth (Ground) conductor and if the Neutral and Earth can be bridged to achieve a zero value. This can be a...

How can the delivery date of this item faster than standard leadtime?

Please check if you can change to AIR shipmode and the delivery date will shorten 7-10 days for AIR transfer.

What is the selection criterion of Circuit Breakers for the Capacitor bank...

The selection should be done after derating the Circuit Breaker taking into consideration voltage variation and capacitors tolerances that could increase nominal current up to 1.5In. The Derating...

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.