Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How convert a 984 HSBY application to Unity
Issue
How convert a 984 HSBY application to Unity

Product Line
Unity

Environment
Windows 10

Resolution
  • Open the ProWORX 32 application.


  • Select the appropriate settings in the 'L984 Options' window.
  • Click on OK


  • The application imported without any errors.   Attempts to rebuild the application will fail with two errors:


This error is expected because the application contains a CHS loadable function block.

The reason for the error is because Unity is not able to delete the CHS loadable block.  The CHS block is not needed in a Unity
Hot Standby application.  The Hot Standby function is managed from Hot Standby window in the PLC configuration.

To resolve the issue:

  • Double click on the error message (This will open the DFB)

User-added image

  • Delete the structured text in the DFB block.

User-added image

  • Rebuild the application.
  • Save the changes.