Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Video: How to add an alarm for Digital I/O with a delay in PME.

Issue
PowerLogic devices with digital I/O alarms do not have the ability to add delays.

Product Line

Power Monitoring Expert (PME) 8.X
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024


Cause
PowerLogic devices such as CM4000 and PM800 devices have the ability to alarm on digital input status changes. Unfortunately there is no way to program a delay into the logic.

Resolution
With PME 8 and later version with alarm configuration we now have the ability to add delays to digital alarms. Adding a delay would make the alarms more consistent with other alarms that have delays built into them.