{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Cannot assign located variable to the Unity Momentum IO
Issue
Cannot assign located variable to the Unity Momentum IO

Product Line
Unity Momentum 171CBU*****

Environment
Unity, Control Expert

Resolution
Located variables cannot be assigned to the Momentum IO as in Concept.

Typically, the hardware configuration information is stored in %KW words for the Unity PLC's.  Due to the hardware
limitation, the use of %KW words is not allowed for the Momentum PLC.  As a result, Unity is forced to use reserved
%MW words for the module configuration information.  The %MW words used for the configuration are intentionally
locked out to prevent the user from changing the values.  This also locks out the the use of a %MW assignment for the IO.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: