{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
The XXMIT 'Retry Limit' parameter (RETRYLMT) does not work on the Unity Momentum PLC
Issue
This resolution describes the issue that occurred with the RETRYLMT parameter on XXMIT Function Block and its solution.


If configuring an XXMIT Function Block in a Unity Momentum PLC using Unity 8.1, 10, or 11, the RETRYLMT function would not work.  Regardless of the value assigned to this parameter, there would be no Retries of the message in the event a communication error occurred.


Product Line
171CBU78090

171CBU98090
171CBU98091

Resolution
The solution to the XXMIT Retry issue is to upgrade the project to Unity 11.1 and update the PLC firmware to version 1.3 IR4.