{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How do I set up a free running timer with a Unity Pro Momentum PLC?
When the project is opened, you will need to double-click the controller to open the configuration window. Check off the Timer Register box and specify the %MW register that is desired for the timer. Build the project and download to the controller.

Below is a video that goes over setting up and configuring a timer register to hold the value of a free running counter, incrementing every 10ms. If the PLC stops the free running timer will stop incrementing.

Schneider Electric Global