{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What actions should be taken if a Unity Momentum PLC exhibits an EC10 or EC00 crash error?

Issue
This resolution explains what actions to take if a Unity Momentum PLC exhibits an EC10 or EC00 crash error.


Product Line
171CBU78090
171CBU98090
171CBU98091


Resolution
The Unity Momentum PLC crash error ‘EC10’ or 'EC00' in %SW124 is resolved by upgrading to firmware versions 2.00 or higher and then reload the program.

It is highly recommended to upgrade to the latest released firmware version.