Nossas Marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como podemos ajudar você hoje?
Downloading the MIB file for version 3 Netbotz.
Issue:
Downloading the MIB file for version 3 Netbotz.

Product Line:
NetBotz v3 Wall Appliance: 355/356 (NBWL0355/6) & 455/456 (NBWL0455/6)
NetBotz v3 Rack Appliance: 450/451 (NBRK0450/1), 550 (NBRK0550), & 570 (NBRK0570)

Environment:
NetBotz version 3 MIB

Cause:
Obtaining the NetBotz version 3 SNMP MIB file

Resolution:

The SNMP MIB for NetBotz Appliances can be downloaded from the NetBotz Appliance itself by accessing the following URL:
*note: If you have HTTP disabled, the url's below will have to be https.

http://ip_address_of_appliance/netbotz300.mib

In versions of Botzware after 3.1.2, the link will be more similar to the version 2 URL

V2:
http://ip_address_of_appliance/netbotzv2.mib

V3
http://ip_address_of_appliance/netbotzv3.mib

The latest MIB should also be available on the APC software downloads page at:
http://www.apc.com/tools/download

It should also be available on the product page for individual NetBotz appliances under the documentation tab.