Are the enclosure dimensions the same for all 8903LG devices regardless of the number of poles?
Issue:
Is the enclosure 8903LG dimension the same for all the devices regardless of the number of poles
Product Line:
Lightning Control and Lightning Contactors
Environment:
Type L/LX Lighting Contactors
Resolution:
Yes, all 8903LO devices use the same NEMA 1 enclosure.
Is the enclosure 8903LG dimension the same for all the devices regardless of the number of poles
Product Line:
Lightning Control and Lightning Contactors
Environment:
Type L/LX Lighting Contactors
Resolution:
Yes, all 8903LO devices use the same NEMA 1 enclosure.
Released for: Schneider Electric Canada