How can we help you today?

What is the the voltage rating of the Class 9999 cover mounted control unit?

Issue:
What is the maximum voltage rating for a 9999 cover-mounted control unit?


Product Line:

NEMA Type S Contactor and Starter Accessories


Environment:

North American Products


Resolution:

The maximum voltage rating for a 9999 cover-mounted control unit is 600 VAC, 50/60 Hz. The contacts carry a NEMA A600 contact designation.

Schneider Electric Canada
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
  • Product Selectors