Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the external operator for the 2510MBW or 2510MCW starter?
Issue:
What is the external operator for the 2510MBW, 2510MCW, 2510MBR, or 2510MCR starter?

Product Line:
Manual Starters and Switches

Environment:
2510 type M manual starters

Cause:
Product Specifications

Resolution:
The replacement external operator is based on the device used and device Series letter. Please note Series is based on enclosed device and not the Series of the open style unit.:

All Series - 2510MBW1, 2510MBW2 and 2510MBW4 as well as 9991MW1 and 9991MW11 enclosures use the 9998HWA1handle assembly kit.

All Series - 2510MCW1, 2510MCW2, 2510MCW3 and 2510MCW5 use the 9998HR3 handle assembly kit.

Series A and Series B - 2510MBW11, 2510MBW12, 2510MBW14, 2510MBW31, 2510MBW32, 2510MCW12, 2510MCW13, 2510MCW15, 2510MCW31, 2510MCW32, 2510MCW33 use the 9998HWA1 handle assembly kit.

Series C - 2510MBW11, 2510MBW12, 2510MBW14, 2510MCW12, 2510MCW13 and 2510MCW15 use the 31085-381-50 external pushbutton kit.

All Series - 2510MBR1, 2510MBR2 use the 9998HR3 handle assembly kit

All Series - 2510MCR1, 2510MCR2, 2510MCR3, and 2510MCR5 use the 9998HR3 handle assembly kit.

9998HWA1 consists of:
Handle Assembly (black/red knob riveted onto shaft)
Rubber Grommet
Retaining Ring
Plastic Washer

9998HR3 consists of:
Handle Assembly (black/red knob riveted onto shaft)
Rubber Grommet
Retaining Ring
Plastic Washer

31085-381-50 consists of:
Complete factory assembled external start/stop pushbutton assembly.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings