Issue:
What is the operating temperature for QO/B and HOM breakers?
Product Line:
Miniature Circuit Breaker
Resolution:
The 10 to 30 A circuit breakers are suitable for use with 60°C or 75°C conductors, while the 35 to 200 A circuit breakers are suitable for use with 75°C conductors only.
What is the operating temperature for QO/B and HOM breakers?
Product Line:
Miniature Circuit Breaker
Resolution:
The 10 to 30 A circuit breakers are suitable for use with 60°C or 75°C conductors, while the 35 to 200 A circuit breakers are suitable for use with 75°C conductors only.
Released for: Schneider Electric Canada