Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are 9999SB Power Poles Convertible from Normally Open to Normally Closed or Vice Versa?
Issue:
Power pole kits for 8903S lighting contactors needs to know if can be field converted.

Product Line:
Lighting Contactors

Environment:
8903 Type S Lighting Contactors

Resolution:
Customer must select the specific power pole, These kits are not convertible.
Ampere
Rating
DescriptionClass 9999 Type
30One N.O.
One N.C.
One N.O. and One N.C.
Two N.O.
Two N.C.
SB6
SB7
SB8
SB9
SB10
60One N.O.
One N.C.
One N.O. and One N.C.
Two N.O.
Two N.C.
SB21 [18]
SB22 [18]
SB23 [18]
SB24 [18]
SB25 [18]


[18] When power pole is added to 60 Ampere contactor, a 4-pole coil is also required.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings