Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the 9999SA2 start stop pushbutton kit momentary or maintained ?
Issue:
9999SA2 operation

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Cover-Mounted Control Units

Resolution:
They are momentary contacts that are meant to be wired into the holding circuit of the starter.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings