Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a QO2150, QO2175, QO2200, QO2150VH, QO2175VH, QO2200VH, or QOB2150VH breaker be installed in a 3 phase load center?
Issue:
Is it possible to install a 2p, 150 - 200 A QO or QO-VH or 2p, 150  A QOB-VH breaker on a 3 phase panelboard or load center?

Product Line:
QO Circuit Breakers

Resolution:
No. The QO2150, QO2150, QO2200, QO2150VH, QO2150VH, QO2200VH, or QOB2150VH branch circuit breakers are two pole breakers that are physically four poles wide and connect to four adjacent connector fingers in the load center or panelboard. They connect to four connector fingers to adequately carry the higher ampacity. If these branch breakers would be installed in a 3 phase load center, a phase to phase short circuit would be created.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings