Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a QO2150, QO2175, QO2200, or QO2225SL be used in a QO three phase load center?
Issue:
Can the 2 pole high Amp QO breakers and sub feed lugs which take 4 spaces be used in a QO three-phase load center?

Product Line:
QO Three Phase Load Centers

Resolution:
NO.
These branch breakers and subfeed lug kit can be applied ONLY in QO, single phase load centers, series G1 or later, rated 150 - 225 A or QONQ single phase load centers rated 300 - 400 A. THEY ARE NOT SUITABLE FOR USE IN ANY QO OR QONQ THREE PHASE LOAD CENTER.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings