How can we help you today?

Where can I find trip curves for the QO-GFI, QO-EPD, and QO-EPE breakers?

Issue:
Where can I find trip curves for the QO/B-GFI, QO/B-EPD and QO/B-EPE breakers?

Product Line:
QO/B-GFI, QO/B-EPD and QO/B-EPE 1P, 2P and 3P Miniature Circuit Breakers

Resolution:
Use the Class 910 trip curves for QO/B-GFI breakers. Though EPD and EPE breakers are not listed on the curve, their trip characteristic is identical to the QO/B-GFI. These curves also apply to the 3P versions of the breakers as well, even though they are not listed on the curve.
Use 910-1 for 15A 1P https://www.se.com/us/en/download/document/910-1/
Use 910-2 for 20A 1P https://www.se.com/us/en/download/document/910-2/
Use 910-3 for 15, 20 and 25A 2P and 3P and 25A 1P https://www.se.com/us/en/download/document/910-3/
Use 910-4 for 30A 1P, 2P and 3P https://www.se.com/us/en/download/document/910-4/
Use 910-5 for 40 to 60A 2P, 40 to 50A 3P https://www.se.com/us/en/download/document/910-5/

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings