Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a two step stored energy mechanism available in the PowerPact P frame breaker?
Issue:
Is a two step stored energy mechanism available in the PowerPact P frame breaker?

Product Line:
PowerPact P frame breakers

Resolution:
Yes, however they are available only as factory installed in a new breaker as the breaker block is different from a standard PowerPact P frame breaker with a toggle mechanism.
Electrically operated P-frame circuit breakers are available only in I-Line and unit mount construction up to 1200 A. These come equipped with a two-step stored energy mechanism and a spring-charging motor.  If a drawout version is required, use Masterpact NT.
Electrically operated P frame breakers contain a spring charging motor (MCH), a shunt trip (MX), and a shunt close (XF), and are available in standard or communicating versions. All 3 items (MCH, MX and XF) must be of the same voltage. An SDE overcurrent trip switch is included.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings