How can we help you today?

What does the S100 designate on Class 2510 Type KGJ2S100?

Issue:
S100 Suffix meaning in 2510KGJ2 Manual starter

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510M Integral Horse Power Manual Starters

Resolution:
This is the standard 2510KGJ2 (jumbo enclosure) with the handle guard/lockout permanently attached. The standard handle guard is secured by screws which can be removed from the outside. This would allow someone to actually remove the locking mechanism. The S100 is provided with the handle guard/lockout pop riveted in place which would require drilling the rivets out to remove the lockout mechanism.