Title:
Motor operated P frame; which electrical accessories are available?
Product Line:
Circuit Breakers
Resolution:
A closing coil, an opening coil, and an SDE contact are standard on a motor operated, PowerPacT P frame breaker. Because it is already supplied, an SDE switch cannot be ordered, nor can the first shunt trip or close coil. A second shunt trip or an undervoltage trip of an optional voltage can be ordered, and up to three form C OF (auxiliary) switches can be ordered. An SD switch, however, is not available on this breaker.
Released for: Schneider Electric Canada