How can we help you today?

What is the degree of protection for the PowerpacT P frame rotary handles?

Product line:
PowerpacT P

Resolution:
The direct mount is IP40 (a little better than NEMA 1) and the door mount is IP55 (like a NEMA 3).

Schneider Electric Canada
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
  • Product Selectors