Issue:
Is there a field installable hand-off-auto selector switch available for the Class 8903 Type LG____ or Type LXG____ lighting contactors?
Product Line:
NEMA Lighting Contactors
Environment:
Products sold and used in the United States
Cause:
Would like to field install an HOA
Resolution:
Yes, order 9999SC2 selector switch and 9999BLX mounting bracket.
Note: On Class 8903 Type LXG the mechanically held contactors it will also be necessary to add CA2SK11** two wire control relay which can be mounted to the side of the contactor using 9999RLX mounting bracket.
** - Complete CA2SK11 part number with volatge code.
Is there a field installable hand-off-auto selector switch available for the Class 8903 Type LG____ or Type LXG____ lighting contactors?
Product Line:
NEMA Lighting Contactors
Environment:
Products sold and used in the United States
Cause:
Would like to field install an HOA
Resolution:
Yes, order 9999SC2 selector switch and 9999BLX mounting bracket.
Note: On Class 8903 Type LXG the mechanically held contactors it will also be necessary to add CA2SK11** two wire control relay which can be mounted to the side of the contactor using 9999RLX mounting bracket.
** - Complete CA2SK11 part number with volatge code.
Released for: Schneider Electric Canada