Issue:
Components for start-stop or on-off pushbutton kit
Product Line:
NEMA Contactors and Starters
Environment:
NEMA Type S Starters
Resolution:
The Class 9999 Type SA3 push button kit consists of two Class 9001 Type K push button assemblies, choice of ``ON-OFF`` or ``START-STOP`` legend plates and fits into two of the three factory provided round knockouts on the enclosure door.
Field Installation:
The Class 9999 Type SA3 will have two, 30mm, Class 9001 Type K push button assemblies, legend plates wiring harness and installation instructions.
Factory Installation:
If the Class 9999 Type SA3 is supplied as a factory modification it is identified as follows:
Form A = Class 9999 Type SA3 using the START and STOP legend plates.
Form A3 = Class 9999 Type SA3 using the ON and OFF legend plates.
Parts List:
(2) 9001 KA1 Contact blocks.
(1) 9001 KN201 - ``START`` legend plate
(1) 9001 KN202 - ``STOP`` legend plate
(1) 9001 KN203 - ``ON`` legend plate
(1) 9001 KN204 - ``OFF`` legend plate
(1) - 9001 KR1B - Black push button operator (N.O. - push to close - spring return)
(1) 001 KR1R - Red push button operator (N.C. - push to open - spring return)
(1) Wiring Harness:
1 Wire = Red, 14Ga, 42`` Long
1 Wire = Yellow, 14Ga, 42`` Long
1 Wire = Black, 14Ga, 42`` Long
Components for start-stop or on-off pushbutton kit
Product Line:
NEMA Contactors and Starters
Environment:
NEMA Type S Starters
Resolution:
The Class 9999 Type SA3 push button kit consists of two Class 9001 Type K push button assemblies, choice of ``ON-OFF`` or ``START-STOP`` legend plates and fits into two of the three factory provided round knockouts on the enclosure door.
Field Installation:
The Class 9999 Type SA3 will have two, 30mm, Class 9001 Type K push button assemblies, legend plates wiring harness and installation instructions.
Factory Installation:
If the Class 9999 Type SA3 is supplied as a factory modification it is identified as follows:
Form A = Class 9999 Type SA3 using the START and STOP legend plates.
Form A3 = Class 9999 Type SA3 using the ON and OFF legend plates.
Parts List:
(2) 9001 KA1 Contact blocks.
(1) 9001 KN201 - ``START`` legend plate
(1) 9001 KN202 - ``STOP`` legend plate
(1) 9001 KN203 - ``ON`` legend plate
(1) 9001 KN204 - ``OFF`` legend plate
(1) - 9001 KR1B - Black push button operator (N.O. - push to close - spring return)
(1) 001 KR1R - Red push button operator (N.C. - push to open - spring return)
(1) Wiring Harness:
1 Wire = Red, 14Ga, 42`` Long
1 Wire = Yellow, 14Ga, 42`` Long
1 Wire = Black, 14Ga, 42`` Long
Released for: Schneider Electric Canada