Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Latching Mechanism Available as a Repair Part for the Class 8903 Type S Mechanically Held Lighting Contactors?
Issue:
The latching mechanism may get worn out or damaged over time.

Product Line:
Contactors and Starters

Environment:
8903 Type S Lighting Contactors

Resolution:
No, if this is damaged it will require replacement of the complete mechanically held contactor.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings