Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a Kirk lock for the Powerpact M P and R frame circuit breakers?
Issue:
Powerpact M P and R frame circuit breakers kirk lock part number

Product Line:
Molded case circuit breakers

Environment:
Powerpact M, P, and R circuit breakers

Resolution:
Order locks from Kirk based on the following information

NOTE: The attached order form contains this information, but this form is only for use when ordering a breaker with a factory-installed keylock.  Schneider does not sell loose Kirk keylocks.
Powerpact M and P frames:
Kirk Single Lock (Horizontal Mount)
Kirk catalog number: KFL003710 add 3 inch roll pin* (old number was SK41683-1)

Kirk Single Lock (Vertical Mount)
Kirk catalog number: KFL003710 (old number was KLF030010)

Kirk Double Lock (Vertical Mount)
Kirk catalog number: KFL003720

Powerpact R Frame:
Kirk Single Lock (Horizontal Mount)
Kirk catalog number: KFL003710 add 3 inch roll pin* (old number was SK41683-1)

Kirk Double Lock (Horizontal Mount)
Kirk catalog number: KFL003720 add 3 inch roll pin* (old number was SK41686-1)

*Horizontal mount Kirk locks on Powerpact P and R breakers require that the lock have a 3" roll pin. When ordering the lock from Kirk, be sure to specifically state "add 3 inch roll pin".

Schneider Electric Canada

Attachment(s)
Kirk Order Form 0613PL0001.pdf [62.56 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings