Is there a three pole QO breaker available that is labeled for 240/120V, similar to the markings on a two pole QO breaker?
Issue:
Application
Product Line:
Miniature QO breakers
Resolution:
The three pole QO breaker is marked for 240 V, but can also be used on 120 V loads if necessary. However, there is no three pole QO breaker available specifically marked at 240/120 V.
Application
Product Line:
Miniature QO breakers
Resolution:
The three pole QO breaker is marked for 240 V, but can also be used on 120 V loads if necessary. However, there is no three pole QO breaker available specifically marked at 240/120 V.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.