What is the torque requirement for the wire in a GS1AW803 lug (#2 - 600 KCMIL) that goes on the 800 to 1000 Amp GS1/GS2/LK3/LK4 switches?
Issue:
Checking on the torque requirement for the wire in a GS1AW803 lug (#2 - 600 KCMIL) that goes on the 800 to 1000 Amp GS1/GS2/LK3/LK4 switches.
Product Line:
GS1, GS2, LK3, LK4 Disconnect Switches
Environment:
Operating Mechanisms and Disconnect Switches
Resolution:
It is 500 lb-in.
Checking on the torque requirement for the wire in a GS1AW803 lug (#2 - 600 KCMIL) that goes on the 800 to 1000 Amp GS1/GS2/LK3/LK4 switches.
Product Line:
GS1, GS2, LK3, LK4 Disconnect Switches
Environment:
Operating Mechanisms and Disconnect Switches
Resolution:
It is 500 lb-in.
Released for: Schneider Electric Canada