How can we help you today?

Are auxiliary contacts available for the Class 8903 Type L electrically held lighting contactor?

Issue:
Are auxiliary contacts available for the Class 8903 Type L electrically held lighting contactor?

Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters

Environment:
North American Products

Cause:
Auxiliary contacts are needed for use with the 8903 type L lighting contactor

Resolution:
We have no auxiliary contacts, per se. Additional power poles must be used for this function. Power poles can only be added to 6 pole through 10 pole devices. Refer to the Digest for additional information.


Schneider Electric Canada
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
Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings