Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the catalog number for a lockoff for a QOT tandem breaker?
Issue:
Is that a lockoff for a QOT tandem breaker?

Product Line:
QO Load Centers

Resolution:
QOTHPA. It can be used to lock one handle in the ON or OFF position.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings