How can we help you today?

Can the operating handle of an enclosed circuit breaker in a P1200S circuit breaker enclosure be padlocked in the ON or OFF position?

Product Line:
Circuit Breaker Enclosure

Resolution:
The operating handle can be padlocked in the OFF position only by purchasing and field installing a S44936 handle padlocking device. The S44936 is considered a removable device. The operating handle can be padlocked in the ON or OFF position by purchasing and field installing a S32631 handle padlocking device. The S32631 is considered a fixed device. The external 9.25 x 9.25 cover plate must be removed to install and use the S32631.

Schneider Electric Canada
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
  • Product Selectors