Issue:
Product Design Features
Product Line:
QO Circuit Breaker Enclosures
Resolution:
The NEMA 1 enclosures, catalog numbers QO2100BNS, QO2100BNF, QO3100BNS, and QO3100BNF, do NOT have a padlock hasp on the cover, BUT each of these catalog numbers comes standard from the factory with the breaker padlock accessory part number QO1PL. The QO1PL is a fixed attachment that goes on the front of the breaker face for padlocking the breaker handle either ON or OFF.
The NEMA 1 enclosures, catalog numbers QO2125BNS and QO2125BNF, DO come standard with a padlock hasp on the front of the cover to lock the circuit breaker handle either in the ON or OFF position.
The NEMA 3R enclosures, catalog numbers QO2100BNRB, QO2125BNRB, and QO3100BNRB, come standard with a padlock hasp that allows the cover to be locked closed. Also, the QO fixed attachment breaker accessory, part number QO1PL, could be used to padlock the breaker handle in the ON or OFF position.
Product Design Features
Product Line:
QO Circuit Breaker Enclosures
Resolution:
The NEMA 1 enclosures, catalog numbers QO2100BNS, QO2100BNF, QO3100BNS, and QO3100BNF, do NOT have a padlock hasp on the cover, BUT each of these catalog numbers comes standard from the factory with the breaker padlock accessory part number QO1PL. The QO1PL is a fixed attachment that goes on the front of the breaker face for padlocking the breaker handle either ON or OFF.
The NEMA 1 enclosures, catalog numbers QO2125BNS and QO2125BNF, DO come standard with a padlock hasp on the front of the cover to lock the circuit breaker handle either in the ON or OFF position.
The NEMA 3R enclosures, catalog numbers QO2100BNRB, QO2125BNRB, and QO3100BNRB, come standard with a padlock hasp that allows the cover to be locked closed. Also, the QO fixed attachment breaker accessory, part number QO1PL, could be used to padlock the breaker handle in the ON or OFF position.
Released for: Schneider Electric Canada