Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we put a 20A lighting contactor inside a MCC Model 6 Standard?
Issue:
20A lighting contactor inside a MCC Model 6 Standard

Product Line:
Type L/LX Lighting Contactors

Environment:
Lighting Contactors


Resolution:
Yes, you can enter as a size 1 starter and omit the overload relay. In special pricing, contact TAG for pricing for lighting contactor. We can install the 8903LO20V20. 0`` additional space, delivery code `F`.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings