Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a QO breaker with ground fault protection at the 50 mA level available?

Issue:
Is there an available QO breaker with ground fault protection at the 50 mA level equipment protection?

Product Line:
Miniature Circuit Breaker

Resolution:
No. The ground fault pickup for QO-EPD breakers is 30 mA, available in 1, 2, and 3 poles. Three pole QO-EPE breakers with 100 mA ground fault protection for equipment are also available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings