How can we help you today?

Can a key lock and padlock attachment both be put on a Powerpact P frame breaker?

Product Line:
Circuit Breakers

Resolution:
You can get both if you order the JE key lock option (factory installed only).  It includes a padlocking provision.

NOTE:
With other key lock options, you can install only one or the other as they both occupy the same space.  This is true for both the electrically operated and standard operated breaker.