Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a shunt trip be added to QO/B or QOU breakers?
Issue:
Are QO/B and QOU breakers available with a Shunt Trip?

Product Line:
Circuit Breakers

Resolution:
Shunt trips can be factory installed only on QO/B, QO/B-SWN, and QOU by adding suffix:
  • 1042 for 12 or 24 Vac or Vdc
  • 1021 for 120, 208, or 240 Vac
The shunt trip terminals accept (2) 14-12 AWG CU wires. The hot and neutral wires can be connected to either terminal. The shunt trip adds an additional pole space to the breaker. If the breaker is ordered without one of those suffixes, a shunt trip cannot be added in the field.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings