{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the torque value for the wire binding screws on PK5GTA?
Issue:
What is the torque requirement for a PK5GTA equipment ground kit?

Product Line:
Ground Bars

Resolution:
#14 - #10 Cu, #12 - #10 Al = 20 lb-in.
#8 Cu/Al = 25 lb-in.
#6 - #4 Cu/Al = 35 lb-in.
Two #14 - #12 Cu, Two #12 - #10 Al = 25 lb-in.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: