Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement reset button for the IEC enclosed LE*D starters?
Issue:
What is the part number for a cover mounted reset button with shaft which manually pushes the reset on an IEC overload?

Product Line:
22mm Operators and IEC Control - GIC Product

Environment:
US Product

Cause:
Product Accessories

Resolution:
The XB5AA86102 is a 22mm pushbutton with shaft which can be used to actuate any LRD3** or LRD** reset button.  This button can be also be used for relays LRD3***, LR2D, or LRD15** units when the adapter part number LA7D1020 is also used.  Mounting depth can be between 17 and 120mm.  See the attached sheet for more information.

Schneider Electric Canada

Attachment(s)
LRD Reset Mechanisms.pdf [783.05 KB]
Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings