Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the correct lugs and wire range for the LK4QU3N disconnect switch?
Issue:
What are the correct lugs and wire range for the LK4QU3N disconnect switch?

Product Line:
LK4 Nonfusible Disconnect Switch,

Environment:
LK4QU3N, 600V, 400A, 3P, terminal lug accessories

Cause:
Clarification of the proper wire range and lug kit to use with the LK4QU3N.

Resolution:
For the Wire range and Lug kits:  Use AWG#4 - 600 kcmil OR AWG (2) #1/0 - 250 kcmil with lug kit GS1AW606 and set screw tightening torque 500 lb-in.  Use AWG # 6 - 350 kcmil with lug kit GS1AW603 and set screw tightening torque 3756 lb-in.
Please refer to the attached drawing of the LK4QU3N.

Schneider Electric Canada

Attachment(s)
LK4QU3N PWCTR-LP67-0012.pdf [56.91 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings