Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the RF limits for QO and HOM breakers with suffixes AFI, CAFI, DF, GFI, EPD and EDB-EPD breakers?
Issue:
RF limits for EDB-EPD​ breakers, and HOM and QO arc-fault and ground-fault protection breakers with suffixes AFI, CAFI, DF, GFI, EPD​​​​​​

Product Line:
Circuit Breakers

Resolution:
All of these products are required to withstand the following:
3 volts/meter radiated intensity between 80 MHz – 1 GHz
3 volts conducted intensity between 150 kHz – 80 MHz

There is a risk of tripping any time the above limits are exceeded.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings