Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to determine if a Powerpact P frame has short or long lugs
Issue:
Which lugs are standard on the Powerpact P frame breakers, and are they short or long lugs?

Product Line:
Circuit Breakers

Resolution:
The standard lug on Powerpact P frame breakers, 250-800 A, unit mount and I-line is the AL800M23K. It is a short lug.
The standard lug on Powerpact P frame breaker, 1000-1200 A, unit mount only is the AL1200P25K. It is a long lug.
The standard lug on Powerpact P frame breakers, 1000-1200 A, I-line only is the AL1200P24K. It is a short lug.
See the below pictures as a reference.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings