Issue:
How do you install a shunt trip or an under voltage relay on a PowerPacT P-frame circuit breaker?
Product Line:
Molded Case Circuit Breakers
Resolution:
Remove the cover by removing the screws on each side of the breaker. Then, connect the connection piece in the designated area of the breaker by screwing it in. You would then install the shunt or under voltage in the slot to the right of the handle, labeled "MN UVR MX SHT". You would align it so that the wiring is coming out of the top left of the device and the silver tab is pointing down from the bottom right of the device. You would then plug the connector into the connection piece. For more information, see the attached instruction bulletin or the instructional video below:
How do you install a shunt trip or an under voltage relay on a PowerPacT P-frame circuit breaker?
Product Line:
Molded Case Circuit Breakers
Resolution:
Remove the cover by removing the screws on each side of the breaker. Then, connect the connection piece in the designated area of the breaker by screwing it in. You would then install the shunt or under voltage in the slot to the right of the handle, labeled "MN UVR MX SHT". You would align it so that the wiring is coming out of the top left of the device and the silver tab is pointing down from the bottom right of the device. You would then plug the connector into the connection piece. For more information, see the attached instruction bulletin or the instructional video below:
Released for: Schneider Electric Canada